Ordering information
For SNLN 30 plummer (pillow) block housings, each of the following items must be ordered separately:
- housing
- seals
- end cover
- locating rings
- bearing
- adapter sleeve
Order example
Two plummer block housings with four-lip seals are required for two 23024 CCK/W33 spherical roller bearings on H 3024 adapter sleeves. One housing will accommodate the non-locating bearing at the end of the shaft. The other housing will accommodate the locating bearing and a through shaft.
The following items should be ordered (in addition to the bearings and adapter sleeves):
- 2 housings SNLN 3024
- 2 four-lip seal packs TSN 3024 (each pack contains two seals)
- 1 end cover ASNH 524-620
- 2 locating rings FRB 12/180